Part Number: TPS65982
Hi Team,
I take TPS65982 as a PD Sink role,when I rewrite the TX Sink Capabilities Register(0x33),how should I update the message to the far-end Source Device?
Now i can do it by used 4CC "HRST" Command,but there is 1 second delay when Hard Rest is going;
Is there any other way faster?
In addition,when i use 4CC "CRST" Command,i can ont see any change on the CC Cable(using the Power Delivery Protocol Analyzer to monitor),it is why?