We have a camera utilizing DS90UB933Q and two deserializer boards - one utilizing DS90UB934-Q1, and the other utilizing DS90UB914-Q1. PCBs are identical, only deserializers are different. When Camera is connected to DS90UB914-Q1 based board everything works fine. If camera is connected to DS90UB934-Q1,based board, image becomes unstable when WiFi router is brought to a close proximity of a coaxial cable connecting camera and deserializer board. What would be the reason for this difference in performance between two deserializers, and is there any way to make DS90UB934-Q1 less susceptible to WIFI interference.