Part Number: PCA9306
Dear Team:
Our customer used PCA9306DCTT the chip to be I2C voltage translator.
Vref1 = 1.8V (Normal)
Vref2 = 3.3V (Standy-by)
When system at S5 (Standby mode) : No1.8V, keep 3.3V,We measured Vref1 leakage voltage around 0.6 to 0.7V:
Customer want to know whether the leakage voltage is normal behavior as this setting condition.
If yes, how to improve it ? customer leakage voltage criterial <0.4V.
Or do we have pin to pin solution can avoid the issue?============================================================
Customer do some testing:
Case(3): R1441 NOPOP, no leakage voltage。
Case(4): R1441 POP 470K ohm, P1V8b leakage voltage (0.6716v)
Case(5): R1439 R1440(470ohm) NOPOP, P1V8b no leakage voltage
Case(6): 把 R1439 R1440(1.2k ohm) POP, P1V8b leakage voltage (0.6537v).
Case(7): 把 R1439 R1440(2.12k ohm) POP, P1V8b P1V8b leakage voltage (0.6383v).