Part Number: DS90UB954-Q1EVM
Dear Sir,
I see DS90UB954EVM or DS90UB954EVM schematics, I found there are caps between hole and ground, can you explain the reason for it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1EVM
Dear Sir,
I see DS90UB954EVM or DS90UB954EVM schematics, I found there are caps between hole and ground, can you explain the reason for it?
I think you have similar issue before. regarding UB954 and UB964, they are similar when visiting different port's device. you can refer to the script in page22 of UB964EVM user guide. also, in UB954 d/s, it is clear on how to visit different port's camera, which is used to differentiate the camera. (set 0x4c = 0x01 for port0, and 0x4c = 0x12 to port1) thanks.
best regards,
Steven