Part Number: DP83867E
Hi,
I'm using the DP83867E to convert from ethernet to SGMII LVDS. I have the evaluation board and measured output signal from SOP. I noticed there was no DC bias on the signal and was wondering why this is the case and how it is achieved given SGMII LVDS spec is supposed to have an offset voltage. Additionally, I have a question about the RJ45 mirror mode, the data sheet states "In some multiport applications, RJ-45 ports may be mirrored relative to one another." is there a specific example of when this is required? I want to use the chip to go from one ethernet port to another via an optical link, does it matter if I enable mirror mode or not? the EVM has worked over the link and mirror mode is enabled on this so I'll stick to this configuration for now but I just want to better understand mirror mode.
Thanks,
Shaun