This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DS280DF810: What are register settings to enable prbs generator and checker using a simple divide by 2, 4, or 8 clock

Part Number: DS280DF810


Using DS280DFxxx or DS250DFxxx we can use a simple divide by 2, 4, or 8 of the data rate clock to generate different prbs pattern at different data rates up to 28Gbps. What are the register settings to make this happen?

  • Enabling PRBS Generator/Checker Through Register Setting:
    The followings are register settings to enable 25Gbps PRBS31 generator on channel 0 and PRBS31 checker on channel 1.

    Note prior to issuing these register settings, make sure we have the following hardware setup:
    1). Turn off output of the clock generator and connect divide by 2,4, or 8 clock to RXP0/RXN0 - using 100-ohm SMA cable
    2). Connect - using differential 100-ohm SMA cable - to TXP0/TXN0 to RXP1/RXN1
    3). Turn power on to the device under test
    4). Turn on output of the clock generator
    RAW FF 03 33 //select channel register and broadcast to all channels
    RAW FC 01 FF //select register set for channel 0
    RAW 2F 40 F0 //**setup every channel to lock to 25gbps
    RAW 60 80 FF //setup device channel 0 and other channels to lock to 25gbps
    RAW 61 BE FF
    RAW 62 80 FF
    RAW 63 BE FF
    RAW 64 FF FF
    RAW 09 04 04 //divider override
    RAW 18 00 70 //divide by 1 since we want to generate highest rate
    RAW 0A 0C 0C //assert cdr reset
    RAW 0A 00 0C //release CDR reset
    RAW FF 01 33 //**enable channel 0 only to generate prbs31
    RAW FC 01 01 //this may not be needed since we already did this earlier
    RAW 2E 04 04 //allow selection of prbs31
    RAW 30 01 03 //enable prbs31
    RAW 1E 10 10 //turn on prbs generator serializer
    RAW 79 00 20 //toggle prbs_gen_en
    RAW 79 20 20
    RAW 30 00 08 //toggle prbs digital clock
    RAW 30 08 08
    RAW A5 80 E0 //select prbs generator on output mux
    RAW FF 01 33 //**check to make sure channel 0 is locked to 25Gbps from channel
    RAW FC 01 FF //select register set for channel 0
    RAW 78 00 00 //check bit 4 if set lock is detected
    RAW FF 01 33 //**enable channel register & don’t broadcast
    RAW FC 02 FF //select register set for channel 1
    RAW 78 00 00 //bits 5 and 4 must be set (sig detect and lock asserted)
    RAW 0D 00 80 //turn on prbs de-serializer for channel 1
    RAW 79 40 40 //enable prbs checker
    RAW 30 00 08 //toggle digital clock
    RAW 30 08 08
    RAW 30 10 10 //force reload of prbs checker seed
    RAW 30 00 10
    RAW 82 40 40 //reset prbs counters
    RAW 82 00 40
    RAW 01 00 00 //check 0x01[6] if set polarity inverted else interverted
    RAW 01 00 00 //check 0x01[4] if set prbs pattern detected
    RAW 01 00 00 //check 0x01[3:0] if equal to 3'b101 prbs31 detected
    RAW 82 80 80 //** check prbs31 error count freeze the current error counter
    RAW 83 00 00 //0x83[2:0] is msb for error count[10:8]
    RAW 84 00 00 //0x84[7:0] is lsb for error count[7:0]
    RAW 82 00 80 //un-freeze prbs error count