Part Number: DS90UB949-Q1EVM
Other Parts Discussed in Thread: DS90UB948-Q1EVM
Hello,
I am using the following evaluation boards:
- DS90UB949-Q1EVM
- DS90UB948-Q1EVM
They are connected by 4 coaxial cables (2 on PORT0 and 2 on PORT1) (each one is 15cm long).
Connection is correctly made between the serializer and the deserializer. I can access their registers using the software Analog LaunchPAD.
But I observe that the CRC Errors counter (register 0x0A-0x0B in the serializer) is constantly increasing (about 4 errors per minute). I do not understand these errors as my set-up is supposed to be very clean, I would say in nominal conditions. Is there a known reason for this phenomenon ?
As I would like to check the connection between the serializer and the deserializer with a far worse link than those 4 coaxial cables, I would like to understand this issue first.
Additional information:
I tested the connection using the BIST mode. I do not have any error on the forward channel (0 on both PORT0 and PORT1 in the deserializer registers). But I still have some errors on the back channel, in both CRC Errors counter (0x0A-0x0B) and BIST BC Error count (0x1B) in the serializer.