Part Number: TPS2500
How will the boost perform if the input voltage is a nominal 5V +10/-18%? What is the expected output voltage range? Will the output through the USB switch be within the +/-10% tolerance of the USB spec?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2500
How will the boost perform if the input voltage is a nominal 5V +10/-18%? What is the expected output voltage range? Will the output through the USB switch be within the +/-10% tolerance of the USB spec?
Thanks!
Hi Bob,
I think this would be good information to have so I am willing to wait 1 -2 weeks for the data.
Thanks!
Hi, Allen,
Sorry for late reply. I just got EVM this week, hope it's not too late. Please see the test result as below. Output voltage is not out of range from the test result.
Device Descriptor Sweep Version Product Name Test Area Package Type Product Revision Test Program Name Meas_Name Test_Parameter Meas_Value Meas_Unit P/F Status Block ID Channel Test Type Start time Lot Station Name UserID Comment Spec_ID Upper Limit Lower Limit Nominal Value Valid End Time Execution Duration (ms) Loop Count Run Mode Name File Path InputVoltage STRING STRING STRING STRING STRING STRING STRING STRING STRING FLOAT STRING STRING STRING STRING STRING DATETIME STRING STRING STRING STRING STRING FLOAT FLOAT FLOAT STRING DATETIME INTEGER INTEGER STRING STRING FLOAT DEV_ID PRODUCT TEST_AREA PACKAGE_CODE PRODUCT_REV PROGRAM TEST_ID TEST_DESC TEST_VALUE UNITS TEST_FLAG FORCING_COND FORCING_COND FORCING_COND START_TIME LOT TESTER OPERATOR COMMENTS FORCING_COND HI_TEST_LIMIT LO_TEST_LIMIT FORCING_COND FINISH_TIME TEST_TYPE FORCING_COND V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.05218308E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642314.271519 C:\ValidationData\Bench\180717111832 4 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.05277548E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642316.149331 C:\ValidationData\Bench\180717111832 4.05 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.05000117E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642318.006145 C:\ValidationData\Bench\180717111832 4.1 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.04617786E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642319.851961 C:\ValidationData\Bench\180717111832 4.15 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.04851734E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642321.727773 C:\ValidationData\Bench\180717111832 4.2 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.04441682E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642323.564589 C:\ValidationData\Bench\180717111832 4.25 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.04442133E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642325.448401 C:\ValidationData\Bench\180717111832 4.3 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.04286202E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642327.304216 C:\ValidationData\Bench\180717111832 4.35 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10257454E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642329.169029 C:\ValidationData\Bench\180717111832 4.4 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10268275E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642331.022844 C:\ValidationData\Bench\180717111832 4.45 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10260271E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642332.886657 C:\ValidationData\Bench\180717111832 4.5 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10263049E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642334.741472 C:\ValidationData\Bench\180717111832 4.55 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10258418E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642336.613285 C:\ValidationData\Bench\180717111832 4.6 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10254906E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642338.440102 C:\ValidationData\Bench\180717111832 4.65 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10254427E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642340.325913 C:\ValidationData\Bench\180717111832 4.7 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10253092E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642342.193727 C:\ValidationData\Bench\180717111832 4.75 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10251985E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642344.057540 C:\ValidationData\Bench\180717111832 4.8 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10254574E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642345.924354 C:\ValidationData\Bench\180717111832 4.85 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10245516E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642347.750171 C:\ValidationData\Bench\180717111832 4.9 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10245578E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642349.625983 C:\ValidationData\Bench\180717111832 4.95 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10244751E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642351.472799 C:\ValidationData\Bench\180717111832 5 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10246394E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642353.350611 C:\ValidationData\Bench\180717111832 5.05 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.10248062E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642355.222424 C:\ValidationData\Bench\180717111832 5.1 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.15230859E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642357.087237 C:\ValidationData\Bench\180717111832 5.15 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.20210045E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642358.946051 C:\ValidationData\Bench\180717111832 5.2 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.25277344E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642360.781868 C:\ValidationData\Bench\180717111832 5.25 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.30255631E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642362.627683 C:\ValidationData\Bench\180717111832 5.3 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.3523965E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642364.524493 C:\ValidationData\Bench\180717111832 5.35 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.40217529E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642366.411304 C:\ValidationData\Bench\180717111832 5.4 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.45199534E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642368.250121 C:\ValidationData\Bench\180717111832 5.45 V TPS2500(no_load) TPS2500.seq Measure_outputvoltage 5.5027428E+0 IGNOREUNIT Passed 17/7/2018 11:18:32 CNX0282722 x0282722 6E+0 4.2E+0 0E+0 0 3614642370.108935 C:\ValidationData\Bench\180717111832 5.5
Regards,
Bob