Part Number: DP83849I
Hello,
I have several boards that are showing 'link-up -100Mbps/Full - flow control off', link-down' swings. The device repeats this continuously.
This happens after the boards have been used for some time. I will leave it connected over the weekend and when I come back I see the behavior.
This is unrecoverable on reset, other boards with the same hardware are fine on the same network connection.
Replacing the phy resolves the issues.(Will need to confirm.)
I am seeing signal on the RX lines, and I occasionally see data on the TX lines. I'm also seeing some <1us pulses on the TX lines, which seems way too fast to be the FLP.
This is all on A, the other port does not seem to be affected. The signal levels look OK.
What would you look at first? What do you recommend as first steps in debugging/ finding root cause?