Part Number: SN65HVD07
1) My encoder send differential data with 5 Volt to SN65HVD7X
2) SN65HVD7X convert to differential data to single data also it decrease voltage to 3.3 V so that my controller are not damaged
3) My microcontroller clock is 3.3 V go to SN65HVD7X (as single line)
4) SN65HVD7X convert 3.3 V single clock (coming from microcontroller) to differential data but still 3.3 V NOT 5 Volt?
My question is about (4. specification) Normally encoder MA+ and MA- should be work master CLOCK (5 Volt ) however it is 3.3 Volt
Can it be problem?
In other words, if I dont use level shifter (3.3 -5 V ) it is problem for my design?
Is there any chip used as both level shifter and tranciver?