Part Number: DS250DF810
Other Parts Discussed in Thread: DS110DF1610
Hi Team,
I working on a new project and need TI help:
DS250DF810 - will it sport CPRI rates 9830.4, 4915.2 and 2457.6 Mbit/s?
Any alternative to MAXP-37161B (16 Channel, 28 Gbps Crosspoint Switch & Signal Conditioner) or similar Crosspoint Switch?
This is the application I need for the upcoming product, I need to support CPRI rate 3~9 and later CPRI 10.
The cross point needs to support:
- FPGA to SFP+ direct connection
- SFP+ to SFP+ CPRI repeater with taping to the FPGA (retimer /DFE ?)
The MAXP-37161B 16 Channel Crosspoint can only support 4 link pairs (I need 6 or 12) and is over flexible.
can you please check what will be the best implementation based on TI chips.
Thanks,
Shlomi