Part Number: DS90UB964-Q1
Tool/software: Linux
Hello,
Hardware system : soc + ds90ub964 + camera(ds90ub913 + sensor)
Image resolution : 1280*720
Problem : camera's fps is 30 fps, but the image received by SOC is only 15 fps.
Whether this is related to the transmission of FPD-LINK?Or do you have any other suggestions?
964's datasheet refers to the following,does this have some influence?
FPD3_PCLK is equivalent to PCLK frequency based on the operating MODE:
10-bit mode: PCLK_Freq. /2
12-bit HF mode: PCLK_Freq. x 2/3
12-bit LF mode: PCLK_Freq.
Thanks!