Hello Team,
I have the pulse output coming from the utility meters such as water meter, gas meter and S0 from Electricity meter.
I would like to interface the pulse output with a radio module which has in built micro controller.
Can you please suggest us the interfacing ICs from the utility meters to the microcontroller?
The challenge here is that the pulse output will vary from 0 to 30V as per S0 specification and there are no specific details on Water and gas meter pulse output.
Appreciate your help!!
Regards, Ramarao