Part Number: DP83867E
When the DP83867E is configured in Analog Loopback mode, is the data that is transmitted just looped back, or is it also transmitted onto the media (MDI)? Section 8.4.4.1.1 of the data sheet says that "While in MII Loopback mode the data is looped back, and can also be configured through register to transmit onto the media." But no similar statement is made for any of the other Near-End Loopback modes. For the embedded testing that I am doing, I need to just have the data looped back and NOT transmitted onto the media (i.e. suppress data to the MDI).
Also, while in Analog Loopback mode, is the PHY isolated from the media, so that it does not receive any messages from the media? Again, I need to ensure that the only messages received while in Near-End Loopback mode are those that I am transmitting (i.e. suppress data from the MDI).
As a side note, I suggest that the data sheet be updated to clarify that the register mentioned in section 8.4.4.1.1 is the BIST Control Register (section 8.6.20). Since MII Loopback mode is selected through the Basic Mode Control Register (8.6.1), it's not obvious which register is used to transmit MII loopback data onto the media (MDI).
Thank you!