Part Number: MAX3243
The Receiver MAX3243CDBG4 has C1+- and C2+-,
These pin have to connect 1uF cap.
What are the function of these pin, and why need cap?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Robert,
This device uses a charge pump to increase, invert, and regulate the voltages at V+ and V- which supply voltage to the outputs. This method requires four capacitors which are external to the device.
C1 acts as a "flying" cap that charges the storage cap at V+ to 5v. C2 is used to invert this voltage and stores it on the cap at V-.
Let me know if you have any more questions.
Regards,
Eric