Part Number: DS90UH949-Q1
Tool/software: Linux
Dear all,
i am trying to have a good image as output on a 1280x480@60 screen from KOE.
The path is : Linux-> HDMI controller -> DS90UH949-Q1 -> fpd link cable (single link) -> deserializer UB928 -> lvds display KOE 1280 x 480
The display timing specs are: 43,2 mhz pixel clock, 40 clk cycles invalid data before the image line, 40 clk cycles invalid after the image line, verticals are 30 lines before the frame, and 20 after.
After some black magic to find proper videomode in linux for this resolution, i have the following result:
The lake image is perfect, even if doesn't seems from the above image, but i am wondering now about the vertical black lines, may be generated by some wrong serializer setting or, i still have to tune better the linux side videomode and blanckings (synch porch etc) ?
Thanks for the support,
Angelo