Part Number: DP83822I
Hi,
Please see the snippet from DP83822I DS below.
"LED pins are automatically configured for the proper polarity based on the bootstrap configuration at power up or hardware reset. If an LED pin is resistively pulled low, the corresponding output will be configured as an active high driver. Conversely, if a given bootstrap input is resistively pulled high, the corresponding output will be configured as an active low driver."
When looking at LEDCFG2, polarity of LED_1 is active low. LED_1 has internally pull down, so shouldn't it be active high? Is the statement above referring to internal or external pull downs/pull ups?
Thanks!
Rgds,
Juha