Part Number: ISO5851
Other Parts Discussed in Thread: ISO5852S, , TIDA-00446, TIDA-00917, TIDA-00195, TIDA-01606
I need to develop an isolated high side gate drive for SiC MOSFET. I am looking for a smart chip that provides isolation, high CM rejection, Desat, Miller clamp, 2 level soft shutdown with the ability to also accept an input from a current sense circuit that if the level from the sense circuit is above a threshold the chip will begin a shutdown or fault. It needs to be able to output if it is in a fault or undervoltage or over temp condition and have the ability for me to reset it. I plan on taking this drive up to 500 kHz so the desat and fault report times need to be fast. I plan on driving MOSFET single modules and half bridge modules in high frequency AC-DC-AC inverters with gate charges around 1100 nC so I will make it a dual channel gate drive with two identical drive circuits on it but isolated from each other. I will use parallel BJT current booster between the smart chip output and the SiC MOS gates. I don't know what TI offers as a suitable chip so I just picked one for the title part number. Any suggestions and reference designs would be greatly appreciated.
Thank you - John