This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH940-Q1: Ask questions about SerDes.

Part Number: DS90UH940-Q1

Hi team

Condition

1. AP Interface: Support for two MIPI CSI-2
2. Connect two cameras.
3. Two images should be continuously monitored by AP and analyzed.

Questions
1. Deserializer IC supports MIPI CSI-2 and serializer should be MIPI CSI-2?
2. If there is 2ch input of Deserializer, can there be a way to output each image simultaneously?
3. Is there any way to use two cameras and one Deserializer? (Condition 2 should be satisfied)
4. I want to play two camera screens at the same time. AP is capable of performance. Please recommend a device that can decode two serial data in real time. (30 frames HD picture quality)

Thanks,

TM

  • Hi TM,
    I think you can select DS909UB954 which can connect two cameras' video input.
    1. dependent on the video format, you can select DVP I/f or CSI2 I/f in the camera side, please read the UB954 d/s
    2. UB954 is one HUB, can support 2 channels video data.
    3. UB954
    4. UB954 can support 2MP camera data. UB964 can support up to 4chanenls video input.

    rgds,
    Steven