Hellow
I am a new user and would like to ask for an assistance:
Below is a scenario that I have to implement:
- Input: A low-frequency logical signal (Din) (up to 50KHz)
- Function#1: to modulate / serialise (Din) into a high frequency of ABT 1GHZ (Differential signal)
- To send it through FIBER
- Function#2: To receive the High frequency and restore/reconstruct back to a logical signal.
- Output: The same input signal (Din) with latency.
Does anyone have an idea how to implement Function#1 and Function#2 ?
Thanks a lot
Gln