Part Number: DS90UB954-Q1
Hi team,
Please tell me the minimum datarate of the FPD-LINK3.
I understand that the maximum is 4.16Gbps and the minimum is 2.0Gbps in CSI-2 mode.
And I think that the maximum is 1.87Gbps and the minimum is 0.7Gbps in RAW mode.
Is it correct?
My customer is considering some combinations such as 913A, 933 and 953.
They would like to check how lowest FPD-LINK frequency can be set because they take care about EMC.
Best regards,
Tomoaki Yoshida