Part Number: TPS65983B
The System:
- TPS65983b
- Aplane Riege SP (JHL6340)
- W25Q80
- Application Customization 3_17
- FW_6.43
The device is a Buspowered Device with additional features which need more power than the 12W. We have an extern power connector which provide us the necessary power. The power connector has an extra pin for the detection for recognized the connection. This pin enables the additional feature.
At the moment the device is a buspowered device which consumes no power if the extern power is plugged.
The detection signal is also route to the GPIO Pin of the TPS65983b. Is there an opportunity to report the Host, that device is now selfepowered?