Part Number: ISO5852SDWEVM-017
Hello:
Recently purchased the EVM to get a system up and running quickly, but found that the schematic in the documentation is unreadable. Is there an Altium design file available? Schematic is needed; PCB not necessary but may be helpful.
Also, the documentation for the EVM (sllu298.pdf) doesn't specify what module is being used in the application note. I'm mating this with one half of a dual Semikron SKM400GB128D IGBT module for switching a 100V, 200A load. Is there anything else that might need to be modified or changed on the module in order to provide a functioning circuit?