Hello,
I would like to design low noise isolated +/-15V rail from 5V input.
Design Requirement :
Vin : 4.5 - 5.5V
Vout : -15V 90mA / +15V 40mA
Since I can't find any transformer for SN6505 from Mouser, Digikey and Farnell,
I decided to use two SN6501 with two transformers.
Do you see any problem with this design?
Can you recommend any transformer for SN6505 with more than 1:1.7 turns ratio and higher current capacity that I can purchase from Mouser, Digikey or Farnell?
Thank you.
EH