Part Number: TUSB1002
hi,
I have some question in using TUSB1002.
The USB3.0 interface used now has USB3.0 switch and Hub on the circuit.
Does this affect the USB3.0 signal? Does it affect the USB3.0 certification test?
In addition, if you add USB1002 to ports near device and Host,
Is it possible to solve the effect of USB switch and Hub?
To meet the USB3.0 certification test.
thanks.