Hello
we want to use XC7027 as ISP which has High 8 bits output of DVP, can we use DS90UB933 as Serializer IC for XC7027?
IF it is ok, so we connect the D0-D7, or D4-D11?
About POC Part, do you Specify the L4 and L7 's suppiler brand?
could you provide the Spec of L4 and L7?
Thanks a lot!