Part Number: DS90UB953-Q1
Please see the questions below. Thanks in advance.
Diagnostics:
- Can voltage (via GPIO0 and 1) and temperature monitoring be performed simultaneously?
- Is it possible to do forward channel diagnostics while streaming? I guess this is done by CRC check?
- Can open or shorted cable be detected with UB953 and UB954 combination?
- Bit-error rate measurement: Can this be performed inside the chip? Or would we need to attach an oscilloscope to measure it?
Best Regards
Joern