This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: 100 Mbps Ethernet Connections, Unused CLK_OUT, & Illegal Strapping

Part Number: DP83867IS

  1. Media Dependent interface connections: please confirm my understanding. I am using this device to operate in 100 Mbps mode. Therefore I will only use one receive and one transmit pair. I want to confirm that my default schematic connections are correct: Port A = PHY output/transmit, Port B = PHY input/receive, Ports C and D are unused. I came to this conclusion by referencing Figure 26 of the TI datasheet and researching the standard pin-out of the RJ-45 connector.

  2. When operating at 100 Mbps, channels C and D of the PHY will not be used. To keep channels C and D I/O in a known state, I plan to tie all four C/D MDI pins to ground, each through a 4.64k resistor. Is this in line with what TI recommends? I couldn’t find anything specific in the datasheet.

  3. If CLK_OUT is not used, can it be left as a no-connect?

  4. Aside from the PHY address strapping, all other strap settings can be controlled by software instead correct? I want to minimize external PHY strapping and let software configure the settings via MDC/MDIO. What about Autoneg Disable? The default Mode 1 state that requires no external strapping does not appear to be a valid mode for the RX_CTRL pin. If I do not strap anything to RX_CTRL (invalid mode for Autoneg Disable control), can software still access/control PHY auto-negotiation enable/disable?

  • Hi,

    If you need is 100M only, have you evaluated DP83822 100M phy ?

    To answer your questions:

    1. Yes, Channel C and D can be left floating or pulled thru ground.
    2. Same.
    3. Clock out can be left NC. You may want to bring it to test point incase you need something for debug.
    4. Yes, straps are controllable thru register configuration. The RX_DV/RX_CTRL
    strap must be configured for strap mode 3 or strap mode 4.The RX_DV/RX_CTRL strap must be configured for strap mode 3 or strap mode 4.

    Regards,
    Geet