This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS254900-Q1: TPS254900-q1

Part Number: TPS254900-Q1

Dear Sir,

We tested TPS254900-Q1 EVM, it was found that even when CTL1 and CTL2 are kept low (operated in client mode), there’s 2.x V on OUT pin.

The following setups.

  1. 12V applied to J1.
  2. Short J2; open J3.
  3. Short pin 3 with pin 4 on J6; short pin 5 and pin 6 on J6.
  4. Around 1.5V was measured on J5’s VBUS pin. (No load is connected on J5)

 Could you help us learn what might be wrong?

Thanks, Ian.