Part Number: SN75DP126
Dear Sir,
Customer met some question while they implement firmware into their BIOS.
As customer feedback, there is no problem to write AEQ registers, but after write data into DPCD register and read back, all they can get is "0".
Is there any method to check if data were be written in registers?
Below are the data they write.
Thanks.
Output Voltage Level (Bit 1、0):
LANE0 --> DPCD 000103h value 10
LANE1 --> DPCD 000104h value 10
LANE2 --> DPCD 000105h value 10
LANE3 --> DPCD 000106h value 10
Pre-Emphasis Level (Bit 3、2):
LANE0 --> DPCD 000103h value 00
LANE1 --> DPCD 000104h value 00
LANE2 --> DPCD 000105h value 00
LANE3 --> DPCD 000106h value 00
AEQ Setting:
LANE0 --> AEQ 05h(BIT 6、4) value 100
LANE1 --> AEQ 05h(BIT 2、0) value 100
LANE2 --> AEQ 06h(BIT 6、4) value 100
LANE3 --> AEQ 06h(BIT 2、0) value 100