This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65MLVD205A: multi-drop configuration impedance termination

Part Number: SN65MLVD205A


Hi,

I would like use SN65MLVD205A with multidrop configuration as below. For sure, Driver output and Receiver input impedances are 100ohm differential. Do I need to put 100 ohm resistor at "T" only? Or, I need to put this 100 ohm resistor at right after the driver output and right before receiver input? Would you please advise about it?

Thanks