Other Parts Discussed in Thread: TUSB9261
I have a new design using the TUSB9260. I noticed that "platform reset" on the design was never going high. Lifting pins one at a time that are connected it turned out to be the TUSB9260. When I lifted pin 4 (GRST) the platform reset signal went high. Do I just have a bad device or is there something internal to the chip that could cause this? This is the first of the 2 protos I powered up.