Part Number: TUSB4020BI
I want set the TUSB4020 into charging mode for a CDP device according to BC1.2
The configuration pins are:
Pin21= (PWRCTL_POL) 4k7 to GND -> active high
Pin36 = (FullPWR) 4k7 to GND -> power switching supported
Pin35 = (Ganged) 4k7 to GND -> individual power control supported
Pin6 = (PWRCTL2) 10k to 3.3V -> battery charging supported
How Can I measure if the TUSB4020 is in battery charging mode by D+/D- lines ?
How can I set the TUSB4020 into a custom charging mode / divider mode for a fixed DC voltage on D+/D- ?
Which register have to be set ?
How can I adjust the voltage ?