Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: DS90UB954-Q1, ALP
We are currently working on the following setup:
Camera <-> 953 Serializer <-> FAKRA Cable <-> 954 De-Serializer* <-> MIPI Adapter* <-> S32V234 EVB2.
MIPI Adapter is connected to De-Serializer through the bottom MIPI connector (J26) on DS90UB954-Q1EVM. To enable this we have populated R60-R69, R71,R72 (0Ω resistors) and R50-R51 (0Ω resistors).
We were trying to validate the output upto De-Serializer by generating a pattern using a code example as mentioned in DS90UB954-Q1 datasheet ( http://www.ti.com/lit/ds/symlink/ds90ub954-q1.pdf ) (Pg No. 63 Section: 7.5.11.4) using ALP.
Can we project the MIPI CSI output into monitor. Is there any TI specific connector(like MIPI to HDMI) for DS90UB954-Q1? Or if there is any other way to debug.