This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LV32E: Is additional TVS needed?

Part Number: AM26LV32E

 Team, 

The AM26LV32EIRGYR provides some pretty good ESD specs.  I’m using this for a quadrature encoder line receiver and there are a number of passive components ahead of the IC inputs.  I’m wondering if I should put another device (TVS) close to the connector pins to better shunt the transients as they enter the board.  I need to be able to accommodate at least 12Mbit/sec, so I can’t have a lot of extra capacitance on the lines.  Is there a TVS part you might recommend for close to the connector pins? Or is this not needed?

Thanks

Viktorija