Part Number: DS25BR150
Other Parts Discussed in Thread: DS25BR110
Hi HSI team,
I have the following questions:
- Can FPD-III be range extended
- How to work with the back channel?
- Seems, it cannot be disabled by software
- Is it in lower frequency range? Could it be filtered out?
- Even better: Can it still be used in extended range? Need of additional bandwidth-limited buffer?
- Is 50m range possible with Cat6a? Gut feeling estimation is just fine J
- How to work with the back channel?
- Can you propose a suitable buffer (Tx) and equalizer (Rx) from the TI portfolio?
- Will DS25BR150/ DS25BR110 work? Need low-cost as we need have two lanes
- What Cat-cable was used for the 15m FPD-III link? How is estimation for a higher quality cable (e.g. Cat x+1)
- Any issues you can think of when running FPD-III at 170MHz PCLK and a 100BASE-TX on the same cable?
Thanks,
Tadeo