Part Number: DS90UB960-Q1
Hi team,
Our customer will use DS90UB960-Q1 for the four camera systems with 953.
All four camera modules are the same, and they want to make the same setting.
They are planning to set up the four camera modules 953 and imager at once in the following way, is this feasible?
・Write data 0x0F to register address 0x4C to allow register write of all FPD 3 ports.
・Write data 0xFC to register address 0x58 to set I2C_PASS_TROUGH_ALL and AUT_ACK_ALL
・Don't set register address 0x5C to 0x6C
Is it possible to access four SERs or imagers by issuing an I2C command from the host to one ID?
Since the camera modules are all the same, the IDs of the four imagers, 953 are the same.
Best regards,
Tomoaki Yoshida