Part Number: DS100KR800
Hello
I have a device operating at 10G that does not tolerate signals on its inputs when un-powered. In order to prevent signalling from reaching the unpowered RX pins, I am looking for a 10Gbps tristatable buffer, repeater or redriver device. I am considering the DS100KR800 for this application. Output tristating needs to be pin controlled, not controlled by SMBUS, so the PDWN Channels register cannot be used. I am wondering if the RESET pin will provide the desired behaviour. Does asserting RESET tristate the repeater outputs?
Regards
James