This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: Back Channnel Disable and FPD-Link III Cable Reach Extension

Part Number: DS90UB947-Q1

Hi Team, 

Is it possible to disable the back channel on the DS90UB947/948? From the datasheet it looks like the back channel has to always be enabled. A customer would like to extend the reach of the cable to over 50m. This app note was referenced: 

http://www.ti.com/lit/an/snla103a/snla103a.pdf

 But it looks like this solution is not possible with the back channel. Another thread was posted here with more information: https://e2e.ti.com/support/interface/high_speed_interface/f/138/t/707723 

If the back channel can't be disabled, are there any other solutions for extending the reach of the cable for this device?

Regards,

I.K. 

  • Hi I.K.,

    The application note you are referencing is for FPD-Link II, which is unidirectional and does not have a back channel.

    The DS90UB947/948 only supports FPD-Link III and would require a back channel to function. These devices are unable to extend the cable over 10m.

    Best,

    Jiashow