Part Number: TPD6E05U06
Other Parts Discussed in Thread: TUSB8041,
Hi,
I'm using TPD6E05U06 RVZ as a USB 3.0 ESD for TUSB8041 device.
According to datasheet, NC pin can be float or connect to GND. In my design, NC pins are soldered on the signal traces. Is it safe or should I modify the PCB so that solder mask covers NC pin area ?
In addittion, what is the best pin assignment for SS signals to reduce the crosstalk between differential pairs ?
In addition, datasheet contains EYE diagram of HDMI application. Can I get the EVE pattern on USB3.0 application ?
Regards,
HeungJun