This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848Q-Q1: Configuration of strap pin

Guru 16770 points
Part Number: DP83848Q-Q1


Hi

Our customer has following questions.

1.

What is the internal pull-up value at PHYAD0?

2.

What is the internal pull-down value at PHYAD1-4?

3.

Do you have information of internal circuit at strap pins?

4.

After the device powered up, some voltage 1.2V - 1.4V is observed at strap pins.

Is it normal?

BestRegards