Part Number: AM26C32
Dear Team,
our customer intends to build a modular PCB that could be used as TX or RX board. To do that, they were wondering if if there is a RX available that has the same pin layout like a TX.
Example: The AM26C32 has
1 - 1A input
2 - 1Y output
3 - 1Z output
A similar TX has:
1 - 1B input
2 - 1A input
3 - 1Y output
Does any TX device exist that has:
1 - 1Y output
2 - 1_ input
3 - 1_ input
Thanks and best regards
Martin