This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26C32: Alternative Pin Layout to be foot-print compatible with TX?

Part Number: AM26C32


Dear Team,

our customer intends to build a modular PCB that could be used as TX or RX board. To do that, they were wondering if if there is a RX available that has the same pin layout like a TX.

Example: The AM26C32 has
1 - 1A input
2 - 1Y output
3 - 1Z output

A similar TX has:

1 - 1B input
2 - 1A input
3 - 1Y output

Does any TX device exist that has:

1 - 1Y output
2 - 1_ input
3 - 1_ input

Thanks and best regards
Martin