Part Number: PCA9306
Hi,
My customer is using PCA9306DCUR for the I2C of HDMI, voltage level is 1.8V and 3.3V. now is having problem of pull-up resistor selection.
When following the selection guide from :
http://www.ti.com/lit/an/slva689/slva689.pdf
condition:
The result is : 900 ohm to 2.95Kohm, selecting the 2.2K.
After using this resistor value, some of the monitor will not work and some will.
This problem become better after increasing the pull up resistor up to 4.7k to 100K ohm.
May I ask if there are other things need to be consider on this case?
Thanks for your help.