Part Number: SN65HVD72
Hi team
About power consumption, my customer want to increase R130 resistance to mega level , is it ok?
The other pull high resistance whether can inrease to 100K?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD72
Hi team
About power consumption, my customer want to increase R130 resistance to mega level , is it ok?
The other pull high resistance whether can inrease to 100K?
Hi Bryan,
To elaborate, fail-safe biasing is a way to give a pin a "default" value when disconnected from other sources. This ensures that when the bus is idle, open, or shorted, or a pin is left floating, the device still behaves in a predictable manner. Because of this, if these pullup resisters are increased dramatically or removed and the device pins are disconnected (or connected to high impedance lines), the device pins will follow the behavior given on Table 1 and Table 2 on the datasheet.
Regarding the increase/removal of the bus pullup resistors (R130 and R137), the device treats the inputs (A and B) as high impedance when the driver is disabled, so if other devices on the same bus are relying on the bus being biased while idling, these resistors should be included.
Regards,
Eric