Part Number: PCA9536
Dear E2E,
We would like to use PCA9536 to control the WP of EEPROM & Flash.
And, We would like to let EE_WP# its default is low in order to let EEPROM can be written.
We are not sure if we need to add a pull low resistor (R530), like as 10K or other value?
in addition, Does SPI_WP still need to pull-high resistor (R529)? (Although PCA9536 already has an internal week pull-high?)
BR,
Jason