This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925Q-Q1: 1 / If DS90UB925Q-Q1 could Compatible with MAX9288 ? or if there any other device could Compatible with MAX9288 ? 2 / I use ds90ub925+ds90ub926 to transfer parallel raw date from senser , the function block as below , if i could use mc

Part Number: DS90UB925Q-Q1


1 / If DS90UB925Q-Q1 could Compatible with MAX9288 ? or if there any other device could  Compatible with MAX9288 ?  

2 / I use ds90ub925+ds90ub926 to transfer parallel  raw date from senser , the function block as below , if i could use mcu to set senser and read flash date through IIC , the IIC host is mcu ,IIC road is mcu--ds90ub926--ds90ub925---senser/flash ?

3 / the senser output is parallel  raw date, the Host mcu input is mipi , If there any project could achieve is , many thanks ~

If DS90UB925Q-Q1 could Compatible with MAX9288 ? or if there any other device could  Compatible with MAX9288 ,many thanks~