Part Number: ISO1541
Hi Team,
In my customer's application, the SCL2 and SDA2 is pull up to VCC2(3.3V) via resistors, what if one of the resistors is short circuit(it means SCL2 or SDA2 is connected to VCC2 directly) and I2C data is in communication status, does the device have risk to get damaged?
Thanks a lot.
Vincent Chen