Part Number: ISO1540
Hi team,
Please let me know some question about spec?
*Capacitive of C1&2
Why are the C1&2 setting the value 40pF/400pF?
In the case of these capacitive over / low, how is the circuit affected?
*Output current side1&2
What is the reason the setting the current value of VCC1/2 are 3.5 mA / 35 mA due to the setting of the pull UP resistance?
And, what is the problem when it gets bigger?
best regards
Hayashi