This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130: SN75DP130 EVM Test 3.3 Pre-Emphasis Failures

Part Number: SN75DP130

DisplayPort PHY Tx Compliance test 3.3 “Pre-Emphasis Level Verification and Maximum Pk-Pk Differential Voltage Testing (Normative)” was run on the TI SN75DP130 EVM. Failures were observed for 0 dB cases. Test 3.3 was initially run without terminations on unused lanes and then with terminations on unused lanes to see if results improved. Both sets of results have failures and are included. The second set also only tests with SSC disabled. Does the TI EVB pass test 3.3 ? If so, are there any special strap or I2C settings required to pass? See attached PDF. TI_E2E_Test-3.3_Draft_v0.pdf